Pre-Turbo PMAC
Discussion about PMAC Products earlier than Turbo PMAC (including PMAC2, PMAC, PMAC-PC, and more) along with their software, including PeWin32, PCOMMSERVER, PCOMM32, and more.
109 topics in this forum
-
- 1 follower
- 9 replies
- 20.9k views
I need license for the following .ocx files. Some seem to be specific to PMAC. These are for VB6 running on ME2000 and I need to install the license on my developer's machine so that we can make some changes for my production machine. Where and how do I obtain license' for these files? And no we aren't going to upgrade. SSTABS32.OCX CTFRAME.OCX BTN32X10.OCX THREED32.OCX PTALK.OCX PTERM.OCX CONTAINER.OCX GRAPHS32.OCX. Thanks in advance as usual
Last reply by warrior, -
- 1 follower
- 1 reply
- 6.7k views
Hi, can anybody help me! A customer has a crashed PC that they use to perform tests of devices but the hard driver has crashed and it can't be recovered and they don't have the original discs. When tring to load a backup version of the software it ask's for a dll called 'pmac.dll'. Part of PMAC User Panel, part of PMAC Motion Control for LabView 5.0 for a ISA slot fibreoptic card (Delta Tau Data Systems Inc. PMAC 2-PC ULTRA-LITE). Looking at 'www.deltatau.com' website, the software there is only for products changed to the PCI format, minus the 'pmac.dll' which I think is for the ISA cards. Do anybody have an ftp site or something similar where I can download or get ac…
Last reply by steve.milici, -
- 0 replies
- 5.3k views
I have a customer using a PMAC2PC104 card and he wants to talk Linux with it. Farooq kindly provided us a file with 2.4 version for a PCI card but my customer is using 2.6 and as Farooq pointed out the PC104 would be an ISA compatible system. I was looking to see if anyone knows of any OEMS, or end customers that might have implemented a Linux driver with a PC104.
Last reply by briansneel, -
- 1 follower
- 2 replies
- 8.2k views
Hi everyone, I am using the PMAC2-PC/104. I want to use the pluse and direction format input with pseudo-closed loop (simulated closed loop). Which variables I should set ? Please tell me if you know. :) Thanks. kalensino
Last reply by kalensino, -
- 1 follower
- 3 replies
- 17.8k views
We have a small stockpile of old PMAC Lite ISA cards that should work (I'm actually in the middle of testing them). These cards are mostly (or all) used cards that were returned from customers during troubleshooting or upgrades, and in most cases there is nothing wrong with the card. Since ISA capable PCs are so hard to find now, we are strongly considering mounting these cards on a homebrew backplane, and using RS-232 to communicate. I have RS-232 communications working on the card on my bench, but I notice that the communication is almost unbearably slow. I removed the E45 and E46 jumpers to set the port speed to 38400, and have changed the port speed in the PCOMM32 …
Last reply by iannicholson, -
- 2 followers
- 8 replies
- 20.8k views
I have several old electric presses, all with Pmac pc 4 channel boards in them. As a part of risk management I bought a used Pmac pc with a pmac pv cpu to have as a swap out replacement just in case. From the limited reading I have done it appears as though it is 8 channel. The question is, if I set the jumpers the same as the old board, load the same firmware as the old board (everything is flash and I have the motion program), download the pmac programs, and plug it in should it work? Thanks in advance
Last reply by steve.milici, -
- 2 followers
- 11 replies
- 26.2k views
Hi! I've got RED LED and GREEN LED at the same time. It looks like whatchdog tripped. The card vintage 1999. Who can help me to solve this problem?
Last reply by Sina.Sattari, -
- 0 replies
- 5.1k views
This calculator aides the PMAC user in setting up and understanding various clock settings. Keywords: Servo Clock PWM Frequency Phase Clock PFM Clock (Pulse and Direction) Encoder Sample Clock Note: Make sure you check Non-Turbo PMAC2 on the upper righthand side.
-
- 1 follower
- 0 replies
- 4.3k views
Several PMAC memory locations are used when generating “machine position” registers for a given application. For axis number one the following registers can be used, M161->D:$0028 ;commanded postion (cts/[Ix08*32]) M162->D:$002B ;actual position (cts/[Ix08*32]) M164->D:$0813 ;position bias (cts/[Ix08*32]) M167->D:$0813 ;master position (cts/[Ix08*32]) M169->D:$0046 ;compensation correction (cts/[Ix08*32]) M174->D:$0840 ;following error (cts/[ix08*32])in memory map! Machine Position = Actual Position + Position Bias + Compensation Correction If using the handwheel offset mode (bit 16 of Ix05 is set i.e. Ix05=$010730) then, Machine Position = Actual Positio…
Last reply by Sina.Sattari,