Machine Vision
246 topics in this forum
-
- 0 replies
- 234 views
The Telnet Client needs to be enabled on Windows for simple "Terminal-style" Ethernet communication with Readers, Imagers or Smart Cameras.Execute the attached WSF File (Windows Script File) and the Telnet Client will be automatically enabled on Windows.You need to perform this operation only once. Operating System Windows 7
Last reply by Omron Forums Support, -
- 0 replies
- 275 views
In some cases, the USB license dongle will lose the Visionscape licensed features (Standard GigE, Intellifind, TPC, DIVS). The reason for this is that each time Visionscape reads the license key, information is written back to the dongle. Non-volatile EEPROM memory eventually fails after some finite number of writes, effectively corrupting the key. This has been fixed in a run-time update to the USB key that allows the key to save license information on the computer instead of the dongle. This runtime has been include in newer versions of the software. Dongles that have lost their licenses will need to be replaced. Contact Microscan for replacement options. To…
Last reply by Omron Forums Support, -
- 0 replies
- 225 views
USB ports go completely dead in sleep mode which disconnects camera. There is a way to keep the USB ports active during sleep mode. Go into Device Manager, navigate down to Universal Serial Bus controllers.On each USB Root Hub item, right-click and choose Properties. Click on the Power Management tab and un-check the box for Allow the computer to turn off this device to save power. Operating System Windows 7
Last reply by Omron Forums Support, -
- 0 replies
- 201 views
Q: Can the original floor stand be used? A: Yes with adapter 98-209441 Q: Do the wires run through the center hole? A: Yes Q: What processor is used in the I-Pak SE system? A: Intel Core 2 Duo Q: Is the UPS mounted externally? A: Yes
Last reply by Omron Forums Support, -
- 0 replies
- 291 views
Before executing the attached WSF File (Windows Script File), you must: - Certify that Telnet Client is enabled on Windows. For more information, please check the article "Enabling Telnet Client on Windows." - Copy the upgrade licenses for the unit to: C:\Microscan\Vscape\Licensing. (You may only have the license for one unit at a time.) - Certify that you have a fresh AutoVISION 4 installation, i.e., just one VSF file available on C:\Microscan\Vscape\Firmware. - Certify that you have correct boot version on the unit. Operating System Any
Last reply by Omron Forums Support, -
- 0 replies
- 174 views
The NL200 series lighting controllers are not UL listed.
Last reply by Omron Forums Support, -
- 0 replies
- 222 views
The NL-200 series is not UL listed.
Last reply by Omron Forums Support, -
- 0 replies
- 177 views
Beyond Trust software will prevent the proper installation of AutoVISION (Visionscape) on a PC. To install the software the following steps must be followed. 1. Logon as an admin account 2. Disable the Beyond Trust services. 3. Reboot 4. Install AutoVISION and reboot. 5. Login as a the same admin and let the installer finish 6. Re-enable the Beyond Trust services 7. Reboot
Last reply by Omron Forums Support, -
- 0 replies
- 190 views
This instruction explains how to remove the filter. WARNING: Removing the IR filter will expose the sensor to environmental conditions. 1. Remove Lens. 2. Remove the two screws, metal plate, and the clear IR filter located inside the lens housing. 3. Re-install the plate and two screws without the IR filter.
Last reply by Omron Forums Support, -
- 0 replies
- 296 views
Telnet to the device IP Address (For ID/MV 30: 192.168.188.2) and Login using VxWorks login : target Password ; password (You will not see the password Echoed on the screen) then at the prompt "->" issue the command: sysConsolePortHelp() + Enter To end your Telnet session at the prompt "->" issue the command: reset. + Enter When you see "Connection to Host Lost" you can then close the window. Operating System Any
Last reply by Omron Forums Support, -
- 0 replies
- 216 views
The attached document provides instructions for the user to switch to different firmware on the MicroHAWK camera. This functionality will require the dual boot license on the camera, in addition to the ID and machine vision licenses. kA23800000007uICAQ_en_US_1.docx
Last reply by Omron Forums Support, -
- 0 replies
- 203 views
In September 2008, Microscan acquired the Siemens Machine Vision group, which through the mergers over the years can be traced back to Itran. Itran is the company developed the MVP 2000T (I-Pak Classic) vision system. In 1999, RVSI Acuity CiMatrix notified all registered I-Pak Classic customers that product support could only be guaranteed through December 2000. At this point Microscan does not provide support for the I-Pak Classic vision system. Microscan has expanded on the capabilities of the I-Pak Classic vision system over several generations of product and currently offers the Visionscape I-Pak vision system to meet the pharmaceutical packaging inspection requiremen…
Last reply by Omron Forums Support, -
- 0 replies
- 209 views
HS-1 Stand 98-000108-01 HS-2D and Mobile Hawk stand 98-000153-01 Contact your Microscan distributor for Pricing.
Last reply by Omron Forums Support, -
- 0 replies
- 231 views
This article is a step by step guide for settings up Microhawk smart camera to send FTP images. It shows how to setup the server side using Filezilla, as well as disable firewall. Please see attached document for a step by step guide on reader setup (=client) and server setup.
Last reply by Omron Forums Support, -
- 0 replies
- 187 views
Before executing the attached WSF File (Windows Script File), you must: - Certify that Telnet Client is enabled on Windows. For more information, please check the article "Enabling Telnet Client on Windows". Attention: This simple package does not check the entered values and does not check if the Dual Boot is installed on the unit! When executed: 1. Enter the MicroHAWK IP Address and click OK. 2. Select the Boot Package Option and the Boot Package Number. 3. Click OK. The ‘lbp’ command is executed. 4. At the "Thank you" message, click OK to close the command screen. Operating System Any
Last reply by Omron Forums Support, -
- 0 replies
- 201 views
NERLITE currently does not offer a SCDI-25 that uses blue LEDs. If you require a blue SCDI then you would need to use: P/N: NER-010304020 SCDI-50 V2, B LED-D, 12V-C, 6 ft. Cbl w/ DB9
Last reply by Omron Forums Support, -
- 0 replies
- 220 views
Attached is a sample calibration certificate for Quadrus Verifier. kA23800000008IDCAY_en_US_1.doc
Last reply by Omron Forums Support, -
- 0 replies
- 197 views
Attached Symbols for Testing: Operating System Any
Last reply by Omron Forums Support, -
- 0 replies
- 230 views
The attached white paper is about using Telnet to reset a Vision MINI or Vision HAWK ConsoleTTY for use with AutoVISION and Visionscape. kA23800000008KYCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 216 views
The Area Arrays with diffusers are no longer available. This is because they were replaced by the Backlight BL series, which will provide more even illumination. To replace the Diffused AR currently used, select the backlight with the same color and similar size, when compared to the AR model.
Last reply by Omron Forums Support, -
- 0 replies
- 180 views
this is a 12V ring light, we no longer sell. the new parts to order for the light and power (US cable) are: NER-011605010 R-60-2, R LED-ND/D, 24V-C, 4.5M (15 ft.) Cbl w/Flying Leads NER-011504100 DSP60 24VDC 2.5A DIN Mount Power Supply NER-030028300 AC Power Cord for DSPxx Power Supply, US
Last reply by Omron Forums Support, -
- 0 replies
- 181 views
This cable is not supported by Microscan. To order a replacement, contact Brent at NTS ntsbrent@comcast.net
Last reply by Omron Forums Support, -
- 0 replies
- 195 views
In AutoVISION 4.0+, connect to the camera and take control (lock) press CTRL-SHIFT-L The License Manager window will open to allow you remove the license from the camera, as seen below. ** DO NOT REMOVE the Machine Vision.lic ** To restore, go to license folder and rename the desired license back to *.lic
Last reply by Omron Forums Support, -
- 0 replies
- 337 views
This procedure intends to provide a very simple way to read output values from Microscan Smart Cameras into an Excel spreadsheet (CSV format). If the output value from the camera contains a comma (as part of a string, for example) it will be treated as a separator and not as part of the read value. In this case, please, use the “Reading Values in Excel (TXT File)” . 1. Reading Text Files in Excel Usually, there are two ways to import data from text files into Excel: delimited text file (.txt) and comma separated values text files (.csv). This procedure presents the use of comma separated values text files (.csv), with the comma character (,) used as the separator o…
Last reply by Omron Forums Support, -
- 0 replies
- 205 views
To do a hard reset if the HS-2D or Mobiel Hawk that is completely locked up: 1. Unplug the reader from the PC. 2. While holding the trigger down, plug the reader into the USB port on the PC. You will hear 5 rapid beeps and then you can let go of the trigger. The unit is now in Boot Mode. 3. To reset the reader, simply hold the trigger down again for approximately 5 seconds until it reboots. The reader will vibrate first and then beep several times and is now reset.
Last reply by Omron Forums Support,