Hello,
I use IDE 4.4.0.99 and want to create a new amplifier with the part manager.
At the end of the section IDE ask for the Power Rating.
What is the meaning of this?
It asked for "Transconduction" in Amps /Volt
Kindly regards part_manager.pdf
Hello,
today I update IDE to 4.4.0.99 hoping that this resolve my problem.
Now it is more worse than before.
With IDE 4.3 I could choose e.g. close or enable in the edit pane.
I press "F1" and could see the information from the manual in the help window.
With the new version this is not possible.
The help window does not open.
I check the point when I got the error pressing F1.
It comes up when I select something in the motor topology window.
Maybe the manual ist not fully linked to the IDE menu.
Kindly regards
Hi,
no IDE in parallel.
I think I did in the past a complete new installation of IDE, not using the patchfile.
Pressing F1 opens a window Microsoft Help Viewer 2.2 - PowerPMAC IDE 4
"Cannot find requested topic on your computer".
Kindly regards
Hello,
just to have quick help "F1" is really helpful, if it works.
But in my installation of IDE it does not work.
What could be the problem?
Best regards
Michael