Jump to content
OMRON Forums

eriochrome

Members
  • Posts

    3
  • Joined

  • Last visited

Everything posted by eriochrome

  1. Seems that the Project I loaded messed up the Powerbrick and I somehow was saving it just as it was dying and the whole usrflash folder was gone on the Powerbrick file system. I loaded a USB with a known good project and placed the files in the usb PowerPmacConfigLoad/usrflash/Project. This recovered communication in the IDE. Once I had communication I tried to reload from one of the flash.n files but that failed also so I am just repeating the basic changes to the project one at a time to source the issue.
  2. Factory Reset USB does not help. I tried the no RT usb and get a different response when I try to run gpascii from the SSH window. With RT I get no response in the SSH window but a flashing cursor on a new line, with NoRT I get a "no such device or address".
  3. I am having a communication problem with my PowerBrick. After building and downloading a new project and saving it something crashed. The IDE stopped being able to communicate with the PowerBrick. I tried the USB Factory reset and have found that the PowerBrick can be SSH to but will not respond to IDE.
×
×
  • Create New...