Jump to content
OMRON Forums

hongluck

Members
  • Posts

    3
  • Joined

  • Last visited

Everything posted by hongluck

  1. Yes it is a Clipper Plus T3 Controller How can I check M602 is correct? , Yes I downloaded suggested M variables It is the same I do not see voltage output with #6O50 command
  2. Hello, I am currently working on Clipper PLUS T3 controller. It is an 8axis clipper . I am using amp 1,2,3 as a milling machine. I want to integrate the spindle to the PMAC Controller and require DAC output. From the thread below I setup I variables. Looked at this thread but could not find an answer http://forums.deltatau.com/showthread.php?tid=185&highlight=spindle+clipper Same as the thread I would like to use DAC output from axis 6. This is what I set I7100=1090 I7101=5 I7102=3 // Output Mode , PWM I7126=0 ; default // Maximum Output I669=1090 ; DAC limit 10 Vdc Then (I600=0 (motor not active)) M602=545 however it did not show 5V. From the manual I found out that output6A(amp6 a output) is pin #4 but is it correct? If I set I600=1 Other pins have Voltage according to the manual but pin 4, 5 is always zero. Can anyone help with this issue?
×
×
  • Create New...