Jump to content
OMRON Forums

cmisztur

Members
  • Posts

    2
  • Joined

  • Last visited

Recent Profile Visitors

The recent visitors block is disabled and is not being shown to other users.

cmisztur's Achievements

Newbie

Newbie (1/14)

  • Week One Done
  • First Post
  • Reacting Well Rare
  • Conversation Starter

Recent Badges

0

Reputation

  1. I have several machines with Geo Brick drives where I need to collect register data near real time. Currently the PC running custom HMI is connected to the drive over USB. I can't seem to find a definite answer in the docs (yet), so I thought to ask it here. Can I create a separate .NET 3.5 application on the same PC and create a secondary connection, through PCommServer, for my purposes to the same drive? Can I make an ethernet connection while USB connection is in use? If so, is this a straight ASCII exchange or do I need to go through PCommServer libraries? Finally, does the RS232 serial port support straight ASCII command-response exchange, without additional libraries (so that I could run my code on a Linux box)? Thank You Chris
×
×
  • Create New...