Hello everyone, I need some help with ACC65E recognization. I'm using a Power PMAC 465 CPU with 4 ACC24E3s and an ACC65E on a 3U UMAC rack. The thing is, ACC 65E cannot be recognized in the IDE, while 4 ACC24E3 are successfully shown. I have switched different slots, but nothing happens.
According to manual, I have set ALL SW1 switches to ON, and then finished the declaration of the pointer as the manual said.
PTR Input1->ACC65E[0].DataReg[0].0.1;
PTR Input2->ACC65E[0].DataReg[0].1.1;
etc.
and
PTR Output1->ACC65E[0].DataReg[3].0.1;
PTR Output2->ACC65E[0].DataReg[3].1.1;
With this fonfiguration, I got "stdin:7:26: Struct Write Gate Part Number Error" when output was written to 1, and "input1=nan" when reading input1.
Is there anything I can do to fix this? Thanks a lot!