teapotbxy
Members-
Posts
7 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Everything posted by teapotbxy
-
ACC65E cannot be recognized by a Power PMAC 465 CPU
teapotbxy replied to teapotbxy's topic in PMAC Technology FAQ
Thank you Steve -
ACC65E cannot be recognized by a Power PMAC 465 CPU
teapotbxy replied to teapotbxy's topic in PMAC Technology FAQ
Thank you for the information! -
Hello everyone, I need some help with the save operation. I'm using a Power PMAC 465 CPU with 4 ACC24E3s and an ACC65E on a 3U UMAC rack. The thing is, "HWChangeErr" and "PwrOnFault" pop up every time the system is powered on, and all the configurations of motors cannot be saved. I have done a save and "$$$" as the following thread said, but the situation stays the same, while the following notices come up in the terminal when executing "save". Is there anything I can do to fix this? I've been stuck on this for several days, could you please give me a hand? Thanks a lot. cp: cannot create regular file `/opt/ppmac/usrflash/Temp/pp_debug.txt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Tools/Tune.tunesetup': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/System/Motors/Motor1.msetup': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/System/Hardware/ACC-65E[0].hwsetup': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/System/Hardware/ACC-24E3[0].hwsetup': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/System/Hardware/ACC-24E2A[4].hwsetup': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/System/Encoder/Encoder.encsetup': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/System/CPU/System.cpusetup': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Log/cpp_error.log': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Log/pp_error_hist.log': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Log/pp_error.log': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Log/pp_proj.log': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/C Language/Include/pp_proj.h': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_save.cfg': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_default.cfg': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_custom_save.cfg': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_startup.txt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_proj.ini': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_disable.txt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_custom_save.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_inc_startup.txt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_inc_disable.txt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/ethernetip_def.eds': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/ethernetip.eds': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/ethernetip.ini': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/ethernetip_def.ini': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/umacro9603977.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/macroio.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/macro2x.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_save.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/geomacro.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/macro1x.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/macro8x.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/macro16x2.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/umacro3603928.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_default.ini': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/macro16x1.tpl': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/filterinfo.flt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_swtbl1.txt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_mro0.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_prog.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_subprog.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_cintelli.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_swtbl1.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_ectcfg.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/IoDrvppmacEcatIO.devdesc.xml': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_global.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_swtbl2.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_stn_mro0.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_swtbl3.txt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_swtbl0.txt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_mtrcfg.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_swtbl3.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_swtbl2.txt': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_hardware.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_swtbl0.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/IoDrvPPMACGlobalIO.devdesc.xml': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_local.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/Database/pp_mrc.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_subprog.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_prog.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_cintelli.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_swtbl1.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_ectcfg.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_global.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_swtbl2.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_mtrcfg.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_swtbl3.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_hardware.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_swtbl0.sym': Read-only file system cp: cannot create regular file `/opt/ppmac/usrflash/Database/pp_local.sym': Read-only file system Successful: SaveConfiguration using /var/ftp/usrflash/Project/Configuration/pp_save.cfg Successful: SaveCustomConfiguration using template /var/ftp/usrflash/Project/Configuration/pp_custom_save.tpl Saving To Flash: Please do NOT Power off until Finished!!! Available disk space = 187757K 2224K Required disk space = 2224K Saving To Flash: Copying files to flash Saving To Flash: Syncing files to flash Saving To Flash: Mounting the flash Saving To Flash: Finished SAVING to flash Save Completed
-
ACC65E cannot be recognized by a Power PMAC 465 CPU
teapotbxy replied to teapotbxy's topic in PMAC Technology FAQ
Thank you Steve, The card has been sent for repair. -
Hello everyone, I need some help with ACC65E recognization. I'm using a Power PMAC 465 CPU with 4 ACC24E3s and an ACC65E on a 3U UMAC rack. The thing is, ACC 65E cannot be recognized in the IDE, while 4 ACC24E3 are successfully shown. I have switched different slots, but nothing happens. According to manual, I have set ALL SW1 switches to ON, and then finished the declaration of the pointer as the manual said. PTR Input1->ACC65E[0].DataReg[0].0.1; PTR Input2->ACC65E[0].DataReg[0].1.1; etc. and PTR Output1->ACC65E[0].DataReg[3].0.1; PTR Output2->ACC65E[0].DataReg[3].1.1; With this fonfiguration, I got "stdin:7:26: Struct Write Gate Part Number Error" when output was written to 1, and "input1=nan" when reading input1. Is there anything I can do to fix this? Thanks a lot!