Under prior versions of the firmware we were able to map to a shared folder on our PC by adding the following lines to the end of fstab:
//192.168.0.100/share /mnt/win cifs credentials=/etc/credentials 0 1
//192.168.0.100/FTS /mnt/FTS cifs credentials=/etc/credentials 0 1
This has worked well for all revisions up to 2.6.0.1, however in the latest FW, 2.6.1.0, the first mount fails and only the second is successful. Adding the _netdev directive to the lines has no effect, however by duplicating the first line to:
//192.168.0.100/share /mnt/win cifs credentials=/etc/credentials 0 0
//192.168.0.100/share /mnt/win cifs credentials=/etc/credentials 0 0
//192.168.0.100/FTS /mnt/FTS cifs credentials=/etc/credentials 0 0
Will now mount correctly, ignoring or erroring on the first mount entry and correctly picking up the next two. While this is an effective workaround, it does not seem like the correct approach and we were wondering why these changes are happening internally to the Linux configuration. It would be much better for us if we could rely on a stable configuration.