I have the code below in a PPMAC script file. It is reporting "syntax error, unexpected SHIFT-LEFT" on the first line that has the <<. The following lines do not report the error. If I comment out the first shift left line, then the next shift line reports the same error. The editor shows the first << as underlined in red showing the error. According to the PPMAC software reference manual, this command should be allowed. Any ideas on what I'm missing here?
// Write flag data to Modbus
temp_byte = rRange200y;
temp_byte << 1;
temp_byte |= rRange200x;
temp_byte << 1;
temp_byte |= rRange100z;
temp_byte << 1;
temp_byte |= rRange100y;
temp_byte << 1;
temp_byte |= rRange100x;
temp_byte << 1;
temp_byte |= rESTOP_Out;
temp_byte << 2;
Sys.ModbusServerBuffer[2] = temp_byte; //load byte