Jump to content
OMRON Forums

luniyasun

Members
  • Posts

    5
  • Joined

  • Last visited

luniyasun's Achievements

Rookie

Rookie (2/14)

  • Conversation Starter
  • First Post
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Never mind. This helped http://forums.deltatau.com/showthread.php?tid=921&highlight=died+waiting+for+longjmp+before+initialization
  2. When compiling a default template IDE project, I get this compiler error. Any ideas what could be causing this? [main] powerpc-405-linux-gnu-g++ 792 fork: child -1 - died waiting for longjmp before initialization, retry 0, exit code 0xC0000135, errno 11 C:\Users\sluniya\AppData\Local\Temp\evtbtoll.fzl\Temp\PowerPmacTest.ppproj 0 1 PowerPmacTest(192.168.0.200) powerpc-405-linux-gnu-g++: vfork: Resource temporarily unavailable C:\Users\sluniya\AppData\Local\Temp\evtbtoll.fzl\Temp\PowerPmacTest.ppproj 0 1 PowerPmacTest(192.168.0.200)
  3. I have a question which is an extension to this. I am using the Power PMAC Component library to create a C# program running on a Windows PC and communicating with PPMAC. What would be the easiest way to access these shared memory data structures as defined in excel through the component library? I can easily access the Power PMAC data structures. TIA ----
  4. I tried to uninstall the previous version of PPMAC IDE in order to update to latest version. The uninstall fails with the following error (screenshot attached). Anybody else facing same problem? Now I cannot run or uninstall old version, neither can I install the new version (gives same error)? Another colleague had similar problems uninstalling the last version of IDE on his computer, that screenshot is also attached Fail.bmp
×
×
  • Create New...