Jump to content
OMRON Forums

ksevcik

Members
  • Posts

    2
  • Joined

  • Last visited

Everything posted by ksevcik

  1. It never occurred to me to run all those values through the ECT just for tuning/charting purposes, so I came up with a hack that works for the plot tool: ECAT[0].IO[1].Data.a - (ECAT[0].IO[1].Data.a & 32768) - (ECAT[0].IO[1].Data.a & 32768) Obviously substitute your values for ECAT[0] and IO[1]. Then use the plot scale factor as necessary to scale to 100% or whatever. It works because to convert from the 16-bit 2s complement, you subtract 2^16 from the unsigned number. The bitwise & picks out bit 15 to indicate sign and subtracts 2^15 twice to convert to the signed form. You have to subtract twice for this to work in Plot Tool. I tried bit shifting or multiplying by two with any number of parentheses and Plot Tool couldn't parse it. Subtracting twice was the only thing that worked. If you wanted to use this in Script or C, this #define should work: #define Torque(value) (value - (value & 32768) << 1) None of these work if you need the torque value available for servo-loop processing or the like, obviously. The ECT would be your only option for that.
  2. I think this is actually a combination of the machine's dynamics and your integral term in the PID loop. Once your Ki builds up an error term, that offset doesn't go away unless you get an opposing error to swing your error term in the opposite direction. The way you're overshooting, you're building up a big error term in the opposite direction that's going to guarantee an overshoot on a move in the other direction, that will.... Here's a step by step of what I think is happening: 1. Motors are killed, error term = 0. You do a step response and your slow Ki doesn't build up a big error term. 2. Motor over shoots slightly on the negative step. While you're waiting around, Ki builds up and error term = +large number. 3. You start another step response. 4. On the positive step, your +large number error term pushes your response into an overshoot. Ki starts reducing the error term until you have little following error, but error term = -large number. 4. On the negative step, your -large number error term pushes your response into an overshoot. Ki starts increasing the error term until you have little following error, but error term = +large number. 5. Go to Step 3. I've actually seen this very thing happen on machines I work on. On a physical machine, there can be enough friction that if you overshoot you need a large integral error term to bring the motor back to 0 following error. That error term makes it it much more likely you'll overshoot in the opposite direction, and then you're stuck in a loop of overshooting. My personal answer is that I don't have to care about that level of error on my machines. I set Ki to 0 and tune my PD and FF terms to get a good low error dynamic response and leave it at that. Considering how small your FE is in counts and in microns, you might take my route. The other possibility (that I haven't tried) is to set your Ki to zero, and tune your Kp and Kd to be well damped with no overshoot. Then start adding in Ki to pull you up to steady state. That way, when you change directions, your error term will damp things even more, making you undershoot and pull up to steady state again. Then you should be in a virtuous cycle of always undershooting somewhat, instead of overshooting a lot.
×
×
  • Create New...