This was posted on the Bugzilla site but the response was that the feature IS NOT supported (uh, but it USED TO BE):
Joe 2013-01-21 13:07:11 PST
A feature that used to work in the v1.4.0.27 firmware is now broken.
Specifically, if you had an M-Variable defined such as:
CycleStopPBOff->Acc65E[0].DataReg[0].2.1; // (CYCLE STOP Pushbutton OFF)
and you attempt to add it to a gather by selecting under a Detailed Plot via
the defined User Globals, you now get the message:
"Acc65E[0].DataReg[0].2.a is not a valid command."
That used to work.
Also, if you attempt to use a previously setup Gather using the same variable,
you will receive the message:
"/var/ftp/gather/GatherSetting.txt:22:17 error #31: invalid function in
equation: gather.addr[15]=Acc65E[0].DataReg[0].2.a UnlinkGatherThread:
root@147.185.x.xxx:/opt/ppmac#"
[reply] [-] Comment 1 Henry Bausley 2013-01-22 08:27:10 PST
(In reply to comment #0)
> A feature that used to work in the v1.4.0.27 firmware is now broken.
> Specifically, if you had an M-Variable defined such as:
> CycleStopPBOff->Acc65E[0].DataReg[0].2.1; // (CYCLE STOP Pushbutton OFF)
> and you attempt to add it to a gather by selecting under a Detailed Plot via
> the defined User Globals, you now get the message:
> "Acc65E[0].DataReg[0].2.a is not a valid command."
> That used to work.
>
> Also, if you attempt to use a previously setup Gather using the same variable,
> you will receive the message:
> "/var/ftp/gather/GatherSetting.txt:22:17 error #31: invalid function in
> equation: gather.addr[15]=Acc65E[0].DataReg[0].2.a UnlinkGatherThread:
> root@147.185.x.xxx:/opt/ppmac#"
You cannot gather a user bit field you must gather the entire register.