Jump to content
OMRON Forums

Joachim

Members
  • Posts

    2
  • Joined

  • Last visited

Joachim's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Thanks, So if i understand right, it' s a Yes. I can configure the geobrick-lv as i' m used to do with a 3phase motor, just change ixx72. Great if it works, we see great potential selling the geobrick with our airbearing rotary stage Best regards Joachim
  2. Hello, Is it possible to run linear motors (u shape) or torque motors which do have only 2 phases? I'm used to work with the Geobrick-lv which is able to run 2 phase motors ( 2phase steppers working fine also 3 phase motors) so it should be a mix of the 2 modes ( stepper and 3 phase brushless) Any idea or tipp? Thanks and Best regards Joachim
×
×
  • Create New...