Jump to content
OMRON Forums

MartinOphey

Members
  • Posts

    12
  • Joined

  • Last visited

MartinOphey's Achievements

Apprentice

Apprentice (3/14)

  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In
  • First Post

Recent Badges

0

Reputation

  1. Is that the right pin configuration?
  2. If i lost the configured ip adress how i can reset it over rs232, which tool is needed?
  3. what is the function behind this two files?
  4. If I include gplib.h in bgcplc I get a lot of errors: Can anybody help me?
  5. How I can save variables remanently?
  6. Is it possible to watch the commanded position before it is filtered by pre-notch-filter? I have programmed a spline move with motion programm to create a asymmetric sine wave. The motion programm spline between sine reference points. If I use the pre-notch-filter the original reference position is not the same like commanded position of motor. I do not want to create a phantom motor for this.
  7. Am I right, that it is necessary to make a power off/on to reset the c written rti code? Also the C-Variables. I have got a feeling that the "$$$***" resets only the the Power PMAC Script Language written code.
  8. Ok, that means there is no way to look c-variable directly?! Because the discribed way takes a lot of time if my code is big and i have a lot of variables.
  9. How I can watch lokal C-Variables form rticplc.c? Regarding the folowing sample: stiffness1 #include #include #include #include #include #include "../../Include/pp_proj.h"const double pi = 3.1415926535;void simulation(void);void realtimeinterrupt_plcc(){simulation(); }void simulation(void){//input variables for simulation double mass, freq1; //output variablesint feedback1;//simulation constantsdouble stiffness1; .... //copy parameters from P-variables to double variables mass = GetGlobalVar (pSimMass); ... stiffness1 = 2 * pi * pi * freq1 * freq1 * mass; feedback1=.... .... //set the simulation output parameters: feedback positions SetPtrVar (mSimMotor1FeedbackPos, feedback1);} Thanks
  10. I need the actual Power PMAC Server. Where i can find it?
×
×
  • Create New...