Jump to content
OMRON Forums

Saurer

Members
  • Posts

    3
  • Joined

  • Last visited

1 Follower

Consent

  • Cookies Consent
    Opt-In

Saurer's Achievements

Rookie

Rookie (2/14)

  • Conversation Starter
  • First Post
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Saurer

    Gantry axis

    I'm trying to setup a simple gantry axis but when switching it off the motor jumps, why? - i have two phantom motors #1 and #2 - all positions are 0 - #1j/#2j/ - #1hmz#2hmz - set Motor[2].CmdMotor=1 - set Motor[2].ServoCtrl=8 - jog #1j=2000 - remove gantry Motor[2].ServoCtrl=1 ==> Motor[2].Pos changes to 0, so I assume the real motor would jump Why do I get a change in position back to 0?
  2. Saurer

    M-Codes

    TURBO2, X8 Firmware version 1.939 We use prog 1000 for reading g-codes and for the movement in &2 (the program has over 2000 lines code), prog 1001 for reading m-codes. Then we use also at same time 3 other coordinate systems (&3, &5 and &12) in time base following mode, master is &2A axis. My problem is: I start all program at same time (&2B0R, &3B42R, &5B43R and &12B45R). I need some settings in &12, it will be set with M-codes. My prog &12B45 goes faster through the code, as I am reading this 15 lines M-code.
  3. Saurer

    M-Codes

    Hello We are using a rotary buffer for G- and M-codes. When we start our program, we fill this buffer at first with one G-Code and then with 15 M-Codes and then again with G-Codes. Now, when I start (run motion prog), then the program "calculated" 10 lines of this M-Codes, make a break and then "eat" the rest of this 5 M-Codes. I have no dwell, while..endwhile, wait statements in my prog 1001. Why my program makes a break after 10 lines? Is this a setting of an I-variable? Or a multitasking problem? Thanks for your help. Regards
×
×
  • Create New...