I am trying to debug a PLC program I wrote for homing all axes connected to a 6-axis GeoBrick, which communicates over USB port to host PC. I am using latest version PEWIN32PRO2.
As the built-in PCL debugger does not seem to work right, I am adding SEND"start home X-axis" statements in my PLC code to figure out where PCL program fails.
When I run PLC program, these text strings are not displayed in the PEWIN terminal window.
I tried all versions: SEND, SENDS, SENDP, SENDR, SENDA and none of them work.
Does the SEND command not work when using USB port?
Same with COMMAND (CMD) command.
Which one do I use for USB port CMD, CMDS, CMDP, CMDR or CMDA.