Here are the 10 serial numbers (They are from the white barcode labels on each of the two boards of each ACC24E2).
1. C0005U28
2. C00068DZ
3. C00068D5
4. C0005U0J
5. C00068B5
6. C0005TXD
7. C00068GK
8. C0005U0M
9. C0005U32
10.C00068DB
Before you do anything with the s/n's, let me update my progress. Hurdle #1 was realizing that there was a different manual for using ACC-24E2 with a power pmac. The 5 ACC24E2 cards (w/opt 1) were addressed according to the ACC24E2 hardware reference (not the 'using with ppmac' manual). Once I figured that out, I was able to see the middle three boards (Gate 1 index i #'s 5,6 and 7). My next hurdle was finding the reference stating that Acc24E2As and E2S's also share the same 'Gate 1 addresses'. Once I removed these two boards, and the address conflict they provided, board #4 was visible in the IDE. So now I can see Gate 1 index i #'s 4,5,6, and 7. My remaining problem is that I cannot see #8 (my fifth Acc24E2 board.) I have taken all of my other boards out of the backplane (with the exception of the CPU and the Power Supply.) (note: I also have qty 2 Acc24E2A, qty 1 Acc28E, qty 1 Acc59E, qty 2 Acc65E and qty 1 Acc84E. Each of these boards has been removed from the rack, so that all that I have installed is the CPU, power supply and qty 5 ACC24E2.)
I have also tried to set SW1 on my fifth board to Gate 1 index i = 9. The board still did not show up.
Also, the 5th Acc24E2 serial numbers are the 1st and 2nd serial numbers listed above.
Any thoughts?
Thanks
- Lane