Hi,
how can I enable the "c-axis mode", if PMAC is in "manual work spindle mode"? I assume that's a machine specific problem. "C-axis mode" means I can control the motor through commands, but it's stiff if I try to rotate it manually. "Manual work spindle mode" means, move commands have no effect on the axis/motor, but I can easily rotate the axis by hand. I checked the value of variable Ix00, but it's 1 in "c-axis mode" and 1 in "manual work spindle mode".
According to the TYPE command, I'm using a PMAC Turbo2. PEWIN gives me that:
TYPE
Turbo2, X8
Help is much appreciated.