Jump to content
OMRON Forums

unreal91

Members
  • Posts

    5
  • Joined

  • Last visited

unreal91's Achievements

Rookie

Rookie (2/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Really thank you for this work. PMAC is working. Already tried and PmacPanel Pro 2. It is also difficult without experience.
  2. Understand the business. I'm building a Machine for the soul in my apartment. I like Deltatau, but money for such purchases not. Perhaps you have available in the archive NC software for my PMAC under Windos XP. Sorry for my English I live in Ukraina.
  3. What program should I use for my case? Where can I download this program, ftp: //support.deltatau.com/DT-USA/? Any help/hints are most appreciated. Best regards.
  4. Hello, DT support. I have the desire to build a simple 3-axes Mill Machine with spindle. I am writing to you for help. I have set: 1. PMAC-PC 602191-104, 4 Axes 2. CPU board Option 2602705-557 (60Mhz) 3. DPRAM, 602240-101 I Have Windows XP In PEWIN-32Pro I fixed the link to the card using IRQ5 (E83 on board), the ISA Bus Base Address Control I/O 021F-0210 (and jmp E66 and E71 's set-OFF), D4000-D7FFF. Motor setup-Ok! DPRAM Test-Ok! I can not create a machine in the PMAC-NC Pro2 Runtime. When you create a project, the PEWIN finds errors in the PLC. Tested, there are variables that are designed for other PMAC. It is possible that PMAC-NC Pro2 Runtime (ver 5.2) is not designed for PMAC-602191 PC-104 or NC5X.phm file? I really hope to help. Will send the necessary files.
  5. Hello, DT support. I have the desire to build a simple 3-axes Mill Machine with spindle. I am writing to you for help. I have set: 1. PMAC-PC 602191-104, 4 Axes 2. CPU board Option 2602705-557 (60Mhz) 3. DPRAM, 602240-101 I Have Windows XP In PEWIN-32Pro I fixed the link to the card using IRQ5 (E83 on board), the ISA Bus Base Address Control I/O 021F-0210 (and jmp E66 and E71 's set-OFF), D4000-D7FFF. Motor setup-Ok! DPRAM Test-Ok! I can not create a machine in the PMAC-NC Pro2 Runtime. When you create a project, the PEWIN finds errors in the PLC. Tested, there are variables that are designed for other PMAC. It is possible that PMAC-NC Pro2 Runtime (ver 5.2) is not designed for PMAC-602191 PC-104 or NC5X.phm file? I really hope to help. Will send the necessary files.
×
×
  • Create New...