Jump to content
OMRON Forums

jkelley

Members
  • Posts

    3
  • Joined

  • Last visited

jkelley's Achievements

Newbie

Newbie (1/14)

  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In
  • First Post

Recent Badges

0

Reputation

  1. Is there any documentation on how to configure an ACC-84E for use with SSI Encoder
  2. CharlesP.. I am still possibly having problems, Here is what I know now Using the ACC-59E section of the manual, Here is my current Configuration ACC-28E --> CS10 Index(0) ACC-65E --> CS10 Index(4) ACC-65E --> CS10 Index(8) ACC-84E --> CS12 Index(1) ACC-59E --> CS14 Index(2) The 28E shows up in the hardware Tree as ACC-28E(0), But only displays the Card Info and Gate Info, Is This Correct? The 84E Shows up int the Hardware tree as well as ACC-84E(1), But it actually displays the Card Info and Gate Info of the Above ACC-28E, Is This correct? The 59E card does not show up in the hardware tree, Its Status Light is on, Is this Correct? Note: I have tried multiple different addressing of this card with the same result
  3. I am having an issue addressing cards correctly. Currently I have a total of 5 ACC24E2 cards, 2 ACC24E2A cards, 1 ACC28E, 1 ACC59E, 2 ACC65E, and 1 ACC84E. I have successfully addressed all of the Axis Interface cards (ACC24E2, and ACC24E2A cards) at Gate1 indexes 4-10. I addressed the ACC28E at GateIO --> 0 (SW1-1 --- SW1-4 are all On) And I can see these through the IDE. The Document titled "UMAC Addresses for I/O Cards" shows switch positions for SW1-1 through SW1-4. The IO Cards also have SW1-5 and SW1-6, and you set these for use in a UMAC, so does the PPMAC just ignore these other two Settings? Can you provide me with switch settings for the rest of the cards? 2-ACC65E's 1-Acc59E and 1ACC84E? And will all of these cards be recognized through the IDE system setup Screen?
×
×
  • Create New...