Jump to content
OMRON Forums

xiaowei506

Members
  • Posts

    1
  • Joined

  • Last visited

Everything posted by xiaowei506

  1. can you use the pmac on the computer(linux), and what is the kernel of linux? [quote='artag' pid='1109' dateline='1295344723'] I'm having some difficulty in using the 'long long' data type on the PPMAC. I'm using IDE 22/07/2010 1.1.1026, firmware 1.2.1.5 and this example code : [code] #include int main(void) { int i; double dd = 0.0; long long ll = 0; for (i = 0; i < 4; ++i) { dd += 1000000001.0; ll = dd; printf("int i %d; double dd %f; long long ll %lld\n", i,dd,ll); } } [/code] I can compile this on another machine (x86 linux), and get the result I expect : [code] int i 0; double dd 1000000001.000000; long long ll 1000000001 int i 1; double dd 2000000002.000000; long long ll 2000000002 int i 2; double dd 3000000003.000000; long long ll 3000000003 int i 3; double dd 4000000004.000000; long long ll 4000000004 [/code] I can also compile it natively on the PPMAC and get the same result. However, if I compile it using the IDE, I get : [code] int i 0; double dd 1000000001.000000; long long ll 0 int i 1; double dd 2000000002.000000; long long ll 0 int i 2; double dd 3000000003.000000; long long ll 0 int i 3; double dd 4000000004.000000; long long ll 0 [/code] I guess this is due to a difference between the cross and native compilers, either due to the crosscompilation or merely an older version. Does the forthcoming IDE release fix this ? -adrian [/quote]
×
×
  • Create New...