Jump to content
OMRON Forums

xiandu

Members
  • Posts

    4
  • Joined

  • Last visited

xiandu's Achievements

Newbie

Newbie (1/14)

  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In
  • First Post

Recent Badges

0

Reputation

  1. Mike, I appreciate that you look into it. You solve my problem!!! Xian
  2. Sina, I use the 'upload' in PEWIN32 to check if the program has been downloaded by the download () function. It looks like the .pmc is not there. Using the 'download' in PEWIN32, the downloaded file appears in the 'upload' program list.
  3. Sina, Thanks. When I download the file within PEWIN32PRO2, it is loaded to buffer and can be run using 'b1r'. I am also sure that i can run the new programmed profile. For example, I have two programs which both use 'OPEN PROG 1' in the codes. Downloading either of them and typing in 'b1 r' will get the respective code running well. Does this answer your questions? I do have a CLEAR after opening any motion program buffer, e.g. 'OPEN PROG 1 CLEAR'.
  4. Hi folks, I need your help with downloading and running a pmc file from my host PC to PMAC. I do programming in VC++ 2005. I cannot run the .pmc file using my C++ code. I tried the function Download() in VC++ as 'pmacDevice.Download(dwDevice,"MOTIONPROG1.pmc", bMacro,bMap,bLog,bDnld,&pbDriverOpen);' I attach the messages that I obtained in the UI of PEWIN32PRO2. I obtain the messages above the blue line when I download and run the 'MOTION PROG1.pmc' within Pewin32Pro2, and obtain the messages below the blue line when I try pmacDevice.Download(dwDevice,"MOTIONPROG1.pmc", bMacro,bMap,bLog,bDnld,&pbDriverOpen). It looks like I did not download MOTIONPROG1.pmc into buffer. When I use '&1b1r', I was running the previous downloaded 'MOTION PROG1.pmc' in buffer. pmcDownloadinfo.PDF
×
×
  • Create New...