Jump to content
OMRON Forums

AhmetNuri

Members
  • Posts

    5
  • Joined

  • Last visited

Everything posted by AhmetNuri

  1. I think I need auto tuninig for my servo drive with adv 400. I read form the adv 400 book, auto tunining need serial connection. I install pmac suit 32 bit. but there is no serial connection settings. there is only ethernet settings. How can I connect adv 400 with pmac suit on seril connection=?
  2. you can wach the video for our servo motor. http://www.2shared.com/video/hsRknapd/delta_tau_tecoservo.html the firest step i use the mpg for motor control. then ı use jog in the video. My old servo motor 1000 rpm and has 5000 ppr encoder. My new servo motor (teko 1 kw with E series drive) 2000 rpm and 2500 ppr . and my old i parameters are i230=5719 i231=5747 i232=6441 i233=16611 i234=1 i235=82902 how can i calculate new i parameter for new drive?
  3. Yes , I have I230, 231,232,232,234,235 paramters.
  4. I see some parameters for motor settings Is any one can explain me what is I230 I231 I232 I233 I234 parameters on the adv 400 ? thanks.
  5. Hi, I have Adv 400 cnc unit. We have a servo motor problem. And we change the servo motor and drive. We use analog mod. I change I230 paramater on the terminal. I can control motor with mpg. it seems normaly. I use Jog mod f5 or f6 motor start work but when the motor stoped 1 or 1/2 cycle turns in the opposite direction. why? the problem is 2. motor. you can see the motor 2 setting from pictures
×
×
  • Create New...