Hi Jimmy,
Thank you for the additional information. The fault did finally clear on the Brick after two days. I used the example code you mentioned, when faulted the temperature values were reading either -45 or 498 degrees, the 8 bit raw data was either 0 or 255. Once the Brick cleared the error it was reading from 29 to 40 degrees. The fault code on the Brick at was 1F5 a couple of times, otherwise it was 3F5, so the fault was evident on both axis 1 and axis 3. The latest error occurred after the Brick was powered up and left idle, the drives were not phased or moving. The error has also occurred when the motors were operating, all of the axis were halted when the error occurred. We are implementing a PLC to monitor the temperatures of the IGBT to better diagnose the issue. The model number of the Brick is GBL4-C0-500-14M00030, serial number is "C0008YSY".
Can you confirm that the maximum average output for this drive is 12 amps? Does that mean that the maximum each axis can draw is 60 percent of the 5 amp continuous rating or 3 amps?
Kind Regards,
John