Charles,
Is there any limitation in terms of the clock rate I can run at on the ACC-5E3 (in this case the Macro Master)? The manual indicate that the values for the Acc5E3[0].PhaseFreq ranges from 35.76 Hz to 2,343,463 Hz. However, when I increased the phase frequency to above 10kHz, the analog readings froze. At the same time, I would think there is a limitation on the clock rate of the ACC-14M as well. Since the ACC-14M has 2 Burr-Brown ADCs that samples at 500kHz at max speed, we would like to run at this speed.
Thanks,
Lei