Currently working with the PPMAC with 24E2A's and could use some advice on the obtaining the following motion profile:
- Use current position as starting point
- Define end point, amplitude, and frequency of motion profile
- Using the above parameters, the robot moves in a sine wave with the overall average path of motion being a linear transition from the start to end point. See attached.
Currently considering PVT mode but would like to avoid defining each curve independently. Any help would be much appreciated.