Jump to content
OMRON Forums

LEDIZES

Members
  • Posts

    2
  • Joined

  • Last visited

LEDIZES's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. We only have a Hall sensor status like: Hall U always 1 Hall V we can see a 0 to 1 slope on the travel Hall W always 0 We also have a Renishaw optical sensor which gives 5000counts per millimeter. Thank you Christian.
  2. I am trying to use a Geo Brick system to drive a ThrustTube 2506 motor, instead of a XENUS drive; the automatic phasing is not possible because the full electrical cycle is 51.2mm, but the real travel on the motor is only around 16mm (so only around 110° instead of 360°); so, is there a procedure to setup the ix91 parameter? Thank you Christian from NBS TECHNOLOGIES
×
×
  • Create New...