Hi!
It's one axis. Did tuning unloaded. IDE-Tune-tool says: NominalGain=4800 (unloaded) resp. 550 (loaded with 21,94 kg)
Servo: 16kHz
RTI: 2 kHz
Topology: Motor #4 and Motor #24 (put-through only) cascaded
Set Adaptive-Control-Parameters:
Motor[4].Servo.NominalGain=4800Motor[4].Servo.EstMinDac=100Motor[4].Servo.EstTime=160Motor[4].Servo.MinGainFactor=1Motor[4].Servo.MaxGainFactor=9Motor[4].Servo.MinW=0Motor[4].Servo.MaxW=0Motor[4].Servo.MinDR=0Motor[4].Servo.MaxDR=0
Put load with 21,94 kg (total of 100 kg possible) on.
Motor[4].Servo.GainFactor remains all time at 1!!
Motor[4].Servo.EstGain wont go above 0.02
Lowering MinGainFactor would lower GainFactor during accel/deceleration equally to MinGainFactor
By the way setting MinGainFactor = MaxGainFactor = 9 would give a nice and stable setup with 21,94 kg load.
I am really rookie-like - but can anybody show me a good practice example?!!
Would I absolutely have to also set MaxW, MinW, MaxDR and MinDR?
Thanks and regards,
Anton