Jump to content
OMRON Forums

gstewartjr

Members
  • Posts

    2
  • Joined

  • Last visited

gstewartjr's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. I think I found answer. The Power PMAC UMAC CPU board can communicate with all of the accessory boards that the older Turbo PMAC2 UMAC CPU board (603766-10x) could use. In addition, it can communicate with a new generation of “PMAC3” UMAC accessory boards for motion, MACRO ring, and I/O that employ a new generation ASIC and a 32-bit data bus on the backplane. Going to try this out. Maybe it is only way to upgrade as PEWIN is not available for download.
  2. Currently have a TurboPMAC2 3U, 4 axis interface, encoder/stepper/ 48 out/ 24in in a rack. Can I replace the TurboPMAC with a PowerPMAC? I'm about to update a customers pmacLite/ISA/Win95 from 20 years ago. It has some PLC programs and ocx communication library? But I doubt I can replicate the win95/ visual basic UI, and purchase communications library. I can't even find PEWIN32 - although it is on customer machine, so I can offload those text based programs. Thanks -Greg
×
×
  • Create New...