Hello all,
I am working on a project upgrading a system from an old PMAC1 card to a newer version. I have very little information (read: none) on the wiring of the amps at the other side of the JMACH1 cable. I am operating under the assumption that the JMACH1 pins are consistent between versions - as such I assume that if I configure the the new card the same as the old one, there shouldn't be a problem. (please, correct me if I am wrong).
I have connected the new card, however when I power up the amps, a loud buzzing sound comes from the back of the PMAC card. Similar to a fan spinning with an obstruction.
I am not sure what could be the cause of this. Is it likely to be mis-configured jumpers? It is a very concerning noise.
OLD PMAC CARD:
VERSION: 1.16D
TYPE: PMAC1, ISA/VME, FLASH, PID, CLK X3
NEW PMAC CARD:
VERSION: 1.17C
TYPE: PMAC1, ISA/VME, FLASH, PID, CLK X2
Regards,
Chris Herring