I test that the maximum file size that can be downloaded and run using a Program buffer is about 10,000.
And I have the same question.When I use the rotary buffer to download and run the program, I can't update the Command position which I used to sending M161.