I'm using a Geo Brick LV 8-axis controller (GBD8-C0-442-10T00000) to drive 5 DC Brush Motors (rating on motor is 30W 24V 2.1A 2000rpm). Since the controller is capable of far more power output than these 5 motors will draw (capabilities listed are 50A peak, 25A continuous, 60VDC Nominal, 80VDC Max), I would like to design a power supply that would allow me to do higher power functions in the future if needed. My questions:
1. Are there any suggestions as to a preferred power supply?
2. I assume the controller is capable of modifying a higher volt supply (say 45V 60V) before sending it to the lower volt motor (here 24V). Is this correct?
3. This project has a limited budget. Would it be advised to purchase a smaller supply that is designed for parallel connection (sized to work for this project) and then purchase additional power supplies to hook up in parallel when future projects arise?