Jump to content
OMRON Forums

Kit Richrds

Members
  • Posts

    4
  • Joined

  • Last visited

Kit Richrds's Achievements

Rookie

Rookie (2/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. I think I only tried using plot once before and it didn't work then. I don't want to try changing versions of the IDE or firmware at this time since the system has just been installed in the field and I don't want to risk breaking it.
  2. I'm trying to use the plot feature of the PPMAC IDE. The gather button seems to work but the upload button never finishes. I have a very simple setup sampling motor 8 actpos, despos, iqcmd, processing motor 8 cmd position, following error. Plotting following error on left axis, cmd position on right axis. Max gather samples 10, sample period 10. The window says Legacy Mode in the lower left corner. Any ideas why it is unable to upload the sampled data? Thanks!
  3. I would like to be able, via the IDE, to set a motor so the homecomplete indication is false. Is there way to do that? PPMAC, ACC-24E3. Thanks!
  4. I need to make schematics and drawings of a system with 26 small motors. I have been given a quote for DeltaTau and Copley equipment to accomplish this but am not finding documentation for some of the Delta Tau equipment. Can someone point me to manuals/drawings for the following? 300-603490-10x Delta Tau AMP-4-1-BP, Analog Amplifier Single Backplane Board. 3-2932A-01-2100-B000 Delta Tau ACC-D3, 21-slot 3U rack. 17.00"Wide x 8.75" Deep X 5.20"High (BLACK plates) 5-4269-00-1821-B0100 Delta Tau Integrated UMAC Rack w/18-Slot Backplane, 21 slot rack & power supply, Black Plates Thanks!
×
×
  • Create New...