Jump to content
OMRON Forums

shekhargalande

Members
  • Posts

    3
  • Joined

  • Last visited

shekhargalande's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. Thank you Sir, I got a reply from support team. I have solved the problem by making I5293=$350C Regards,
  2. Please can anyone provide help on the above as the matter is urgent and i have only one day left. Thanks in advance
  3. Below are the setting done for Phantom Axis. Phantom axis moves in Jog modes but the Time base does not start. -Setup Phantom Encoder Table: -below motors 1 – 8 setup for Clipper TurboPMAC2 hardware -M9 is setup to integrate the commanded position register for M9 $0488 I8008=$280488 Motor 9 entry 1 Unfiltered Parallel pos of location Y:$488 (M961->$D0488 #9 Cmd Pos) I8009=$18000 Motor 9 entry 2 I8010=$4803509 Time Base Entry with Encoder 9 as master I8011=1350 Time base rate I5293=$350C or $350A ;Make Virtual Encoder as master for C.S. 2 I5294=8388607 ;Max Slew Rate ;I8012=$0 End of Table
×
×
  • Create New...