Hello,
I'm trying to develop a Python application that will control the Turbo PMAC2 and some other devices.
This Turbo PMAC2 is installed inside a machine, and works very well with PWin32Pro2.
I'm trying to use a dll to do this, is this the best option?
I downloaded a lot of Turbo PMAC2 manuals, and I found the PComm32PRO manual:
http://www.deltatau.com/manuals/pdfs/PCOMM32%20PRO.pdf?id=635415374139453187
But a think it's obsolet, it talks about the PComm32.dll, and some examples that should be in the library, but it doesn't exist. I found just the PComm32W.dll and PcommServer.exe (that starts when I try to open a communication with PMAC2).
These two, PWin32PRO2, are installed by PMAC Executive Pro2 Suite.
Sometimes my application works, and I can read and change the value of a P variable(it was all that I could do until now), but it's totally unstable. It just works when it wants.
Is there a new manual or a example about how to do this?
Is a dll the best option?
*I can not uninstall PWin32PRO2. The machine must work in the both options without reconfiguration.
**The conection is USB.
Thank you!