RomanSolonto
Members-
Posts
27 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Everything posted by RomanSolonto
-
Power clipper doesn't run after firmware updating.
RomanSolonto replied to RomanSolonto's topic in Power PMAC
I tried to create "PowerPmacFirmwareInstall" folder and put powerpmac465 2-4-0-180.zip and 2.1.1.3 powerpmac465.zip (packed and unpacked). Nothing happens. -
Power clipper doesn't run after firmware updating.
RomanSolonto replied to RomanSolonto's topic in Power PMAC
The firmware version is 2-4-0-180. I tried to enable pmac with inserted usb disk (Folder PowerPmacFirmwareInstall was created). 2.1.1.3 powerpmac460ex from file depot. Nothing happens. Only green led and enabled fan. -
Good afternoon. We have the power pmac clipper board. We updated the firmware. We made an update through Power pmac IDE. During the update download, the connection was broken and the controller stopped loading. We checked the drive with the file system by loading it on a similar board, it was the pmac clipper board too. We think that the problem is the damage to the firmware of the FPGA. We tried to restore the firmware through USB. The controller does not read USB-drive. The controller also does not read the flash drive where the operating system (Linux) is located. We tried to create the folder "PowerPmacFactoryReset" on the USB drive and run the power pmac clipper. It doesn't work. Clipper didn't read USB-flash at all. Now when we start the clipper, it turns on green led and nothing more. Tell me how we can restore the boot firmware to turn the pmac clipper and fix board boot.
-
Greetings. Turbo PMAC clipper. I have a trouble with M163 (motor number is one) variable when controller processes the cnc program. When controller processes positive (more than 0) move command it works fine. But when controller processes negative move command it doesn't work at all! For example. I load this program: T1 F3200 G0 X40000 (target position is 40,000) X0 (target position is 0) X-40000 (target position is 0 ...) X0 (target position is 0). Why is the target position displayed incorrectly?
-
Good day. NC has some functions to work with the desired line number: SearchLine SearchText SearchTextNext. The next procedure is working: PHMIDoc.SendCmd("Devices.PmacNC1.SearchLine(0,25)") Desired line changes. But PHMIDoc.SendCmd("Devices.PmacNC1.SearchText(0,""N20"", 0)") Does not working. Desired line not changes. There is the form "frmSearch" in NC. ''frmProgramMenu" has the next procedure: Public Sub Search() Dim MyStr As String MyStr = "Devices.PmacNC.Search" PHMIDoc.SendCmd(MyStr) ... ' frmSearch.Show 1 ... End Sub "frmSearch.Show 1" is commented out. It looks like it was used in earlier versions of the program. "Devices.PmacNC.Search" shows dialog box that i don't like. Procedure "btnSearch_Click" of the "frmSearch" does not working too: Private Sub btnSearch_Click() Dim MyStr As String Dim m_MatchCase As Long If (chkMatchCase.Value = True) Then m_MatchCase = 1 Else m_MatchCase = 0 MyStr = "Devices.PmacNC1.SearchText(0,""" + txtSearch.Text + """," + Str(m_MatchCase) + ")" PHMIDoc.SendCmd (MyStr) btnSearch.SetFocus txtSearch.SetFocus End Sub How can I search text and set the desired line without dialog box that used "Devices.PmacNC.Search"
-
I have some Turbo Umacs with Axis Expansion Boards and I/O boards. can I change only processor modules to upgrade the CNC systems? Or Power UMAC and Turbo Umac are not fully compatible?
-
I am confused by the line from Power PMAC Clipper User Manual.pdf: Clipper[0].Chan[2].OutputMode = Clipper[0].Chan[2].OutputMode & ( Clipper[0].Chan[2].OutputMode ^ 8 ) You can record easier: Clipper[0].Chan[2].OutputMode &= $07 But the DAC worked need set to 1 third bit Clipper[0].Chan[2].OutputMode? Then need: Clipper[0].Chan[2].OutputMode |= $08
-
I have plate POWER Clipper with Option 12. I use 4 servo motor with direct PWM control. Need DAC output. I write setup: Sys.WpKey = $AAAAAAAA; Clipper[0].PhaseFreq=10000; Clipper[0].PhaseClockDiv=0; Clipper[0].ServoClockDiv=3; Clipper[0].AdcAmpStrobe=$fffffc Clipper[0].Chan[2].PwmFreqMult=5 Sys.PhaseOverServoPeriod=1/( Clipper[0].ServoClockDiv+1) Sys.ServoPeriod=1000*( Clipper[0].ServoClockDiv+1)/Clipper[0].PhaseFreq Clipper[0].Chan[2].OutputMode= Clipper[0].Chan[2].OutputMode&( Clipper[0].Chan[2].OutputMode^8) I'm trying to read the value from Gate3[0].Chan[2].Pwm[3], but get 0. What am I doing wrong?
-
Output by structure doesn't work (bgcplc0)
RomanSolonto replied to RomanSolonto's topic in Power PMAC
Tried PPScriptMode and EnumMode: 1. // #define _PPScriptMode_ #define _EnumMode_ 2. #define _PPScriptMode_ // #define _EnumMode_ But the result is not changed - on the output port has no signal. What else could prevent the loading of a number in a variable Gate3[0].GpioData[0]? -
Output by structure doesn't work (bgcplc0)
RomanSolonto replied to RomanSolonto's topic in Power PMAC
I use POWER CLIPPER -
Output by structure doesn't work (bgcplc0)
RomanSolonto replied to RomanSolonto's topic in Power PMAC
Ok, I corrected the variable types: // Local variables: #define adrMvar 3000 unsigned int modAdr = 0xFFF000FF; // Template variable unsigned int adr = 0; // Create a pointer to a structure: volatile unsigned int MyFirstICAdr; volatile unsigned int *MyFirstICGpioData; MyFirstICAdr = pshm->OffsetGate3[0]; // Gate3[0] MyFirstICGpioData = (int *) piom + ((MyFirstICAdr + 0x250) >> 2); // Defined pointer on Gate3[0].GpioData[0] // Read the value of the M-variable with a type cast and mask overlay: adr = ((int) GetPtrVar(adrMvar)) & 0x0000000F; // Modify a variable and pass it to the registry I/O Gate3[0].GpioData[0]: modAdr |= (adr << 16); // The result will be the following, when adr=0xf (for example): adr<<16 = 0xf<<16 = 0xf0000; modAdr = modAdr | 0xf0000 = 0xFFF000FF | 0xf0000 = 0xFFFf00FF pshm->Gate3PartData[0].GpioOutData[0] &= modAdr; *MyFirstICGpioData = pshm->Gate3PartData[0].GpioOutData[0]; But the result is not changed - on the output port has no signal. Includes the following files: #include #include #include #define _PPScriptMode_ // uncomment for Pmac Script type access #define _EnumMode_ // uncomment for Pmac enum data type checking on Set & Get global functions #include "../../Include/pp_proj.h" #include Need to connect something else? -
Good day. // Local variables: #define adrMvar 3000 int modAdr = 0xFFF000FF; // Template variable int adr = 0; // Create a pointer to a structure: int MyFirstICAdr; int *MyFirstICGpioData; MyFirstICAdr = pshm->OffsetGate3[0]; // Gate3[0] MyFirstICGpioData = (int *) piom + ((MyFirstICAdr + 0x250) >> 2); // Defined pointer on Gate3[0].GpioData[0] // Read the value of the M-variable with a type cast and mask overlay: adr = ((int) GetPtrVar(adrMvar)) & 0x0000000F; // Modify a variable and pass it to the registry I/O Gate3[0].GpioData[0]: modAdr |= (adr << 16); // The result will be the following, when adr=0xf (for example): adr<<16 = 0xf<<16 = 0xf0000; modAdr = modAdr | 0xf0000 = 0xFFF000FF | 0xf0000 = 0xFFFf00FF pshm->Gate3PartData[0].GpioOutData[0] &= modAdr; *MyFirstICGpioData = pshm->Gate3PartData[0].GpioOutData[0]; // As a result, the outputs of MO1, MO2, MO3, MO4 (it Gate3[0].GpioData[0].16.4) must appear, but it does not appear
-
Power Clipper's multiplexed port protocol datasheet
RomanSolonto replied to RomanSolonto's topic in Power PMAC
Thank you. I'll try -
Power Clipper's multiplexed port protocol datasheet
RomanSolonto replied to RomanSolonto's topic in Power PMAC
I need a device whose dimensions do not exceed 190x110 mm with 16 inputs and 16 outputs. Is it real? -
Good day. I have Power Clipper and I need to use multiplexed port. I have some design constraints and I can not use the standard ACCs. Where an I find the detalied information about JTHW port?
-
No channels in "System setup" (Power Pmac IDE, Power clipper)
RomanSolonto replied to RomanSolonto's topic in Power PMAC
I have 2 Clippers. The problems are simmilar. first: Gate3[0].PartType 618089 Gate3[0].PartOpt0 $ffffffff Gate3[0].PartRev 15 Gate3[0].PartType 15 barcode C000FR2A second: Gate3[0].PartType 618089 Gate3[0].PartOpt0 $ffffffff Gate3[0].PartRev 15 Gate3[0].PartType 15 barcode C000GJ2Z -
No channels in "System setup" (Power Pmac IDE, Power clipper)
RomanSolonto replied to RomanSolonto's topic in Power PMAC
Thank you. But there is one strange thing. In other Power Clipper ( it was "one of the original Power Clippers" http://forums.deltatau.com/showthread.php?tid=2323) it worked at the same versions of the firmware. Now I can't use alias "Clipper[0]", only "Gate3[0]". Is it normal? -
Sys.NoClocks error after PowerClipper firmware upgrade
RomanSolonto replied to RomanSolonto's topic in Power PMAC
Previous firmware version was 1.6.0.119. S/n DEUP-08GI21C1T ASSY 604050-100 Vers 2.1.1.3 Power clipper. "2.1.1.3 powerpmac465.zip " was used. In Errors monitor I have: Sys.Gate1AddrErrDetect = 0x5554 Sys.NoClocks = 1 How can I capture "boot response"? Can it be captured only from serial port? Thank you. -
Good day. I'd download new firmware (2.1.1.3) on PowerClipper. IDE version is 2.2.0.39. When I start IDE I receive error Sys.NoClocks and Sys.ServoCount is 0. Before updating Sys.ServoCount was updating.
-
PWM signal on DAC (like Clipper's Option-11A)
RomanSolonto replied to RomanSolonto's topic in Turbo PMAC
Hi, I have Turbo Pmac (not Clipper) and I need to control the output power of the laser. I tried to use countdown timer to create PWM signal. NCAutopilot creates this PLC: I make: where m4602->Y:$78E08,0,12,U ; DAC ch#1 P1011 and P1012 - time for countdown timers But I have some problems: 1. Frequency not stable 2. I think that it's not right way. Is there any way to control frequency and duty cycle? Is it possible to use PWM control of amplifiers for this? -
Hi, I have Turbo Pmac (not Clipper) and I need to control the output power of the laser. I tried to use countdown timer to create PWM signal. NCAutopilot creates this PLC: I make: where m4602->Y:$78E08,0,12,U ; DAC ch#1 P1011 and P1012 - time for countdown timers But I have some problems: 1. Frequency not stable 2. I think that it's not right way. Is there any way to control frequency and duty cycle? Is it possible to use PWM control of amplifiers for this?
-
How can I find where this theme was continued?
-
GetVectorVelocity() (current feedrate) in PLC
RomanSolonto replied to RomanSolonto's topic in Turbo PMAC
Thank you very match.