Hi,
To use the whole table I need to put I226 on -9000000 but then it do not find the zero position of the sensor with the home command.
If I put I226 on -8000000 there is no problem.
Is there a limit for Ix26?
peter
Thanks ,so for the same machine it is always the same set of sub- programs ? sorry it is all new for me.
So the code of the Cam program I put after the sub programs ?
peter
I have a x-y table that a use for woodworking a PMAC PC card and everthing is working with simple programs that I write myself.
To use G-code (CAM program)with my card a need to translate it to pmac code.
Is it necessery to add the "translation" for every program ?
as far as I understand G03 jumps to program 1000 where stands do "linear "
But it are always the same "translations" so can I store them on the card or so.?
peter