Jump to content
OMRON Forums

kebitmatf

Members
  • Posts

    4
  • Joined

  • Last visited

kebitmatf's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. Actually, I don't know well which pin should I use. Please give me a suggestion!
  2. Actually, I don't know well which pin should I use. Please give me a suggestion!
  3. Dear Everyone, I'm using Model Clipper T1 to control a motor that is scan a sensor in a line. During the moving of the motor, the sensor is getting data at each interval distance (scanning resolution). To do this, 1 output pulse from the clipper will trigger the sensor to get 1 signal. I'm using the PCOMM32.DLL in Visual Basic 6.0. But, I don't know what is the command used to control the pulse output. Could someone help me to solve this problem?
  4. Dear Everyone, I'm using Model Clipper T1 to control a motor that is scan a sensor in a line. During the moving of the motor, the sensor is getting data at each interval distance (scanning resolution). To do this, 1 output pulse from the clipper will trigger the sensor to get 1 signal. I'm using the PCOMM32.DLL in Visual Basic 6.0. But, I don't know what is the command used to control the pulse output. Could someone help me to solve this problem?
×
×
  • Create New...