Jump to content
OMRON Forums

macs

Members
  • Posts

    2
  • Joined

  • Last visited

Everything posted by macs

  1. Hi all, I know that I can access global variables that I defined in 'global definitions.pmh' by pshm->P[variableName] in C, but this doesn't work for global array by pshm->P[arrayName(index)]. I know there must be a way to access them, please is there are somebody can tell me? Thank you!
  2. macs

    Error messages

    Hi, When I was trying to build and download a project that contains only codes files that are generated by Simulink-Power PMAC Interface, the error messages appeared: C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : make: *** /opt/powerpc-465-rootfs/usr/src/linux-3.2.21-serengeti-smp: No such file or directory. Stop. Actually I can build the same project without error messages at another computer which is not connected to a PPMAC. And I also tired to reinstall the PPMAC IDE, when I first ran it in 'No Device' Mode, I could successfully build it. But after I connected to the PPMAC, I can't build it again anymore, even in offline mode. Here are the error messages appeared when I build the same project in offline (No device) Mode: C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_printf' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_fwrite' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_fprintf' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_puts' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_free' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_fputs' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : collect2: ld returned 1 exit status Could somebody help me, please?
×
×
  • Create New...