Jump to content
OMRON Forums

Kaydon Steve

Members
  • Posts

    1
  • Joined

  • Last visited

Kaydon Steve's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. Hi I'm new to this forum and am a rookie to PMAC programming and set-up. I have two machines, very simple each with a single axis, connected to a control box (built and set up by a third party) which contains a PMAC2 controller. The first unit has been working just fine for about 2 years, then the PC that runs the operator interface (Labview-based) was upgraded to WIN 7. I had to reinstall the PMAC software. Had problems, but eventually figured out I had to upgrade the USB driver and got it working again. Everything OK now, EXCEPT, that I need to change a few I-variables (130 thru 134 and 902). Using Pwin32PRO ver 4.4.0.0 I change the variables and everything is great. But when I shut down the input power (440 volt) for maybe an hour or so, some of the changed variables revert to their original setting. I'm also building a second machine just like the first, and its PC also has WIN7. New install for all the software etc. and it has exactly the same problem. I assume the problem must have something to do with the WIN7 change, but can't figure out how to solve it. Any help would be much appreciated. thanks
×
×
  • Create New...