Thank you very much for your reply.I tried with your suggestions.Following are the observations.
I checked the value of I19 it is 7207, i4900 is showing $4 from this I can say it is a Servo IC number 2, this number is matching to I19 of 7207.I checked the value of i7207 it is zero from this i can say it is internal generation of phase clock and internal generation of servo clock.
I corrected the counting direction of simulated encoder pulses as per the motor shaft movement. Even i7216 value is 3 then it is a DAC output. I made i180=0. after all this my observations are DAC output is continuosly coming with 0.7 volt. In global status window i observed there is a error with Servo/Macro config error. after giving a command of #1J/ again the "Attempt to perform phase reference during move, move during phase reference, or enabling with phase clock error" is coming. our amplifier fault signals are status+,status- , this is a digital output but axis interface pins having analog fault inputs ,can i bypass the giving of fault input status to UMAC. please give the suggestions