Jump to content
OMRON Forums

Yiven

Members
  • Posts

    6
  • Joined

  • Last visited

Yiven's Achievements

Apprentice

Apprentice (3/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Hello, can some body give me the firmware which is Turbo1 V1.947 (11-01-10). Thanks
  2. Hello, can some body give me the firmware which is Turbo1 V1.947 (11-01-10). Thanks
  3. The BrickAC.STO 0/1 can be used in Brick AC controller to monitor the Safe Torque Off status, does these BrickAC.STO 0/1 commands can be used in Power Brick LV also?
  4. What is the best way to connect with Power PMAC by the Mac laptop (Ex. Telnet etc...)? Is any way Ex. Socket library can be used to communicate with Power PMAC?
  5. My system is power brick with the trust driver, I do the Amp/Motor setup(7 steps) via IDE system setup, and all the steps seems work fine, then through the last step (Test and Commission the Motor) try to turn run the motor, but it not work. I just saw the trust driver can be servo on after I click the Test button, but the motor can't be turn run even not holding(free), I measure the Analog voltage command from the power brick Amp connector, the voltage is 0, is any problems or process I missing? Ps: The trust driver just do the amplifier function, and the commutation is done by power brick.
  6. My previous controller is Turbo Brick controller with the using CFG file. Now, I have to update my current control system from Turbo to Power Brick. Does the Turbo Brick using CFG file still compatible with the new Power Brick controller ? If, No. How/Which variables I have to change? Thanks
×
×
  • Create New...