Jump to content
OMRON Forums

JamesJennings

Members
  • Posts

    3
  • Joined

  • Last visited

JamesJennings's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Would it be safe for the acc59e to combine multiple unipolar DAC outputs together in parallel so as to avoid the expence/ complexity of a switching matrix? The idea is that normally only one dac channel at a time would be commanded with the others set to zero. I don't want the combined output added just the value of the highest Dac output at any given moment.
  2. Where can I find this pdf file? I'm having the same problem. I'm sure its in my not setting the buffer chip direction but I can't find the power pmac address for it (acc5e manual only addresses turbo)
  3. I need to do the Equidistance Pulse output per traveled distance along a path using turbo UMAC. Any examples to follow? Also would it work instead of using position compare on a phantom axis to use the output of an unused acc24e2a axis set up as an open loop stepper motor in follower mode? Could this achieve higher pulse rates? I'm mostly a hardware guy. My programming skills are modest. Examples would help.
×
×
  • Create New...