Hello,
I'm programming several GeoBrick-LV controllers.
While I succeeded in doing the basic setup and moving motors and creating simple PLCs, I still don't know if I got all the M-Variable definitions right.
My first idea was to use the definitions from the software reference manual, p. 610 (TURBO PMAC2 SUGGESTED M-VARIABLE DEFINITIONS). But the Geo Brick LV's manual gives different definitions for the GPIO related variables (p. 36). Now I could just replace the definitions of GPIO-related M-Variables, but how can I be sure, that there are no further differences?
When I tried to download the suggested definitions via PEWIN32
(Configure->M-Variables->Download Suggested M-variables)
it seems to load definitions as given in the software reference manual, which are different from the GeoBrick LV manual suggestions, for example:
M0->Y$78400,0
M1->Y$78400,1
....
from the SRM vs.
M1->Y$78800,0,1
M2->Y$78800,2,1
....
from the GeoBrick LV manual.
Can you provide a full list of suggested M-Variables for the GeoBrick LV?
Best regards,
Christoph