I have installed Power PMAC as administrator, I have entered an IP on startup so it will link to a VM. This is all ok but when the Power PMAC Suite opens the Terminal window is not working and the Watch window causes a crash if you try to remove the Sys.ServoCount command. Also the watch window seems to always have a windows loading mouse cursor.
I have reinstalled many times but I still get the same issues every time I start Power PMAC up and connect it to a VM.
PC Specs:
OS: Win 7 Pro 64-bit
CPU: Intel Core i-7-3840QM 2.8GHz
RAM: 8GB
SSD drive with ample space