Jump to content
OMRON Forums

seanxyuan

Members
  • Posts

    4
  • Joined

  • Last visited

Everything posted by seanxyuan

  1. Our system was working properly but we cannot connect to Power PMAC controller any more. We get the following message: "Can not add the device 192.168.0.200 to network route". One of our PCs is still able to connect but the other one cannot. Is it related to windows automatic update maybe? Has anyone faced the same issue before? This is urgent. I appreciate your help.
  2. Thanks for your response. I set Coord[1].SegMoveTime=10 and still it moves linear not circular. Is there any other parameter that I should change to have a circular move for X and Y?
  3. I am trying to create a circle move (1 quarter - 90 degrees) using the prog1.pmc code as below: undefine all &1 #1->1711025 X #8->1365276 Y #2->2105867 Z #7->393216 a open prog 1 ta 125 ts 35 tm 1000 dwell 2000 G17 G91 G02 X0.25 Y0.25 I0.25 J0.25 close For G-Code commands, I have also created subprog1.pmc as follow: open subprog 1000 N0: rapid return; N1000: linear return; N2000: circle1;return; N3000: circle2 return; N9000: dwell 10 return; N17000: normal K-1 return; N18000: normal J-1 return; N19000: normal I-1 return; N90000: abs return; N91000: inc return; close However, the output is just a LINEAR movement from current position to point (0.25,0.25). I tried several other ways, such as using circle1 directly in my prog1.pmc but none of them worked. Can anyone help what might be the issue here? Thanks,
  4. Were you able to solve this issue using Paramiko and Python3?I am also able to run commands like "ls" but when I send the ''gpascii' command it hangs there. Any suggestions?
×
×
  • Create New...