Jump to content
OMRON Forums

glennstanley

Members
  • Posts

    5
  • Joined

  • Last visited

Everything posted by glennstanley

  1. With the assistance of your support staff via telephone, we have concluded that the Geo Brick AC internal amplifier has failed. Unit does not replay to ampver ampmod only produces and error message. The unit is being prepped for rma Thanks.
  2. My problem continues. RY gets me 0. No change. I see PEWin32Pro2 reports in the terminal header Terminal: Device #0 [QMAC TURBO]V.1947 I think it be "GEO Brick Drive" instead of QMAC. What do I do now? How do I confirm it might REALLY be a QMAC?
  3. I attempted to phase using #1$ RY gets me 0 I tried #1o0 and get "attempt to perform phase reference during move, move during phase reference, or enabling with phase clock error" This is a GBL4-CO-505-??D We attempted hardware RESET on outside of GEO Brick chassis These LEDS are under the (D10) 7-segment display There are 4 LEDS. I don't have a WD (Watch Dog) glowing LED This config file was running for some time until now. It is in the field. I don't have any LIMITS set for any axis.
  4. ...Can’t phase a thing Yet there are no limits on any of axes 1-4. I can't remember how to poke register Y:$002014. tried with MVar M1000->Y:$002014 but that does not work I also tried RESET LED INACTIVE and +5 are glowing My customer reports that he does not see anything on 7-segment (D10) display Also did $$$*** I also cycled power.
  5. Brick responds with E0000000 error after attempt to phase any axis. However, no axis has limits violation. Could this be a runt-time error of sorts?
×
×
  • Create New...