Jump to content
OMRON Forums

spark

Members
  • Posts

    3
  • Joined

  • Last visited

spark's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. Hello Unit101, sorry to disturb you again, I'd like to know whether PMAC send bytes one by one to serial port, or all bytes at one shot. Thanks for your time!
  2. Oops!I have made the elementary mistake, the address is a HEX number. thanks a lot, @Unit101! You have done me a great favor.
  3. Hello everyone: I'm using a turbo PMAC2 CPU, and I have a serial devices need to interface with the delta tau(receive some HEX data from PMAC). The problem happened as follow: I'm trying to a set of HEX numbers like "00 01 02 03 04 05 06 07 08 09 0A 0B 0C 0D"(14 numbers in total),all these values are assigned to the M-variables from M0-M13, the PLC program are listed blow. --------Begining of the program------- CLOSE I52=5 ;Basic setup to enable auxiliary serialport I53=15 ;Baud rate is set to 115200 I1 = 1 I43 = 3 M100->X:$FFFFE1,24 ;The number of bytes to output M101->X:$FFFFE3,24 ;Starting address to send M102->X:$FFFFE0,23 ;bit 23 of X:$FFFFE0 must be set to 1 to enable the output M0->Y:$3600,0,8 M1->Y:$3601,0,8 M2->Y:$3602,0,8 M3->Y:$3603,0,8 M4->Y:$3604,0,8 M5->Y:$3605,0,8 M6->Y:$3606,0,8 M7->Y:$3607,0,8 M8->Y:$3608,0,8 M9->Y:$3609,0,8 M10->Y:$3610,0,8 M11->Y:$3611,0,8 M12->Y:$3612,0,8 M13->Y:$3613,0,8 OPEN PLC1 CLEAR M0=$00 M1=$01 M2=$02 M3=$03 M4=$04 M5=$05 M6=$06 M7=$07 M8=$08 M9=$09 M10=$0A M11=$0B M12=$0C M13=$0D M101=$3600 M100=13 M102=1 DISABLE PLC 1 CLOSE" ------End of the program--------- But I received a string "00 01 02 03 04 05 06 07 08 09 00 00 00 00", then, I changed the value of "M100" to "19", and I received a string "00 01 02 03 04 05 06 07 08 09 00 00 00 00 00 0A 0B 0C 0D 00", I'm curious about this output, why does five 0 Byte appear? anyone could tell me what happened? Thanks a lot!
×
×
  • Create New...