Jump to content
OMRON Forums

ltremblay

Members
  • Posts

    3
  • Joined

  • Last visited

Everything posted by ltremblay

  1. Well, I thought I was good by installing everything from zero (4hrs...), removing key registers, appdata, ... until I've start to add ENI file from system config. I've got a beautifull freezing window and communication loss with pmac... Note that I also try to use V3.0 of pmac ide before to have problem (but I don't thinnk that this is the problem).
  2. Hi unit101 ! Thanks for your answer. Your asumption where right. I finally manage to make it work but now I'm back on this problem. It is probably related to the fact that I try to update ec eng (v2.5 vs 2.8) to solve an other problem related to ESI... Now as soon as I try to connect with ec eng, the communication between pmac and IDE crash... I also received a beautifull pop up stating : "Failed to configure Marster-unit: Time-out (ErrCode : 0x98110010)"... Unforgotly your step to resolve this problem didn't work. When I go with ec eng. without passig with pmac with network that I know where working: All good. I will uninstall everything and install back to see if my little finger was right.
  3. Hi, I try to push my ethercat configuration embeded in an eni file generated by software ec eng. Problem stated in setup message of ethercat system setup: MasterState is in Unknown mode please type "ecat reset" in terminal window. This command don't seem's to exist command, I only have ecat resetSafety. Can you help me on this ?
×
×
  • Create New...